Can not change write community string for NBRK0750, NBWL0755
Published date:
29 October 2019
Issue:
Can not change NetBotz version 5.2 write community string.
Product Line:
NetBotz
Environment:
NBRK0750, NBWL0755
NetBotz 5.1, 5.2
Cause:
The write community name is only used when working with StruxureWare DCE at this stage. It was added in as a default to be able to work with DCE's priority scanning feature.
The UI was not initially updated to allow for editing of this field.
Resolution:
Version 5.2.1 is slated to have an edit field for this setting.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.