Which NetShelter SX cabinet has a greater cable capacity, 750mm wide or 800mm wide?
Published date:
31 May 2019
Issue:
A customer asks if the 800mm wide NetShelter cabinet has a larger cable management capacity.
Product Line:
NetShelter SX
Environment: All versions and serial ranges.
Cause:
A customer is trying to choose 750mm vs. 800mm wide cabinets.
Resolution:
The 750mm wide and 800mm wide cabinets use the same vertical cable managers so they have the same cable management capacity.
For example; AR7580A is the high volume vertical cable manager used in AR3150 and AR3350, and also in AR3180G and AR3380G.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.