SRT 8 or 10kVA experiences excessive battery transfer and re-transfer events in 3 phase systems
Published date:
18 September 2018
Issue: The UPS experiences excessive battery transfer/retransfer events in 3PH systems.
Product Line:
SRT 8-10kVA Models
Resolution:
Clear the Alarm. Turn the output ON again. If the problem persists, Brain dead the UPS. If the alarm reoccurs, perform a UPS Firmware upgrade to the latest 04.7 revision that addressed these issues. For complete upgrade instructions please refer to FA164737.
Release Notes (UPS 04.7):
========================
1. Improved system performance of transitions between Online and Bypass operation modes. 2. Improved system behaviour for three phase input configurations to reduce transitions to battery under certain input feed conditions.
3. Improved system behaviour to eliminate false detection of DC bus under voltage alarm under certain conditions.
4. Improved system handling for certain AC input conditions during system start-up.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.