How can I change my pump rollover timer settings in my Motivair pump package?
Published date:
24 January 2019
Issue:
How can I change my pump rollover timer settings in my Motivair pump package?
Product line:
All Motivair Dry Coolers Eaton 500 PLC controllers.
Environment:
All Serial Numbers.
Cause:
Install, Repair.
Resolution
This controller can be changed through the display.
Setting Changeover Timers:
The changeover timer is set with the buttons on the front of the Easy Relay. Changeover is measured in Hours. To adjust the Changeover timer, press OK, then use the Up or Down arrows to highlight Parameter. Press OK and O1 is selected. Press OK again. The first digit in O1 is selected. Press OK again. The cursor changes to a blinking digit. Press the right arrow to move the cursor over to the digit to be changed. Use the Up or Down arrows to adjust the value of the selected digit. Once the desired changeover time has been set, press OK, then press Esc three times.
NOTE: Factory Default Program has a 7-day (168 hours) pump rotation/changeover timer setting.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.