Browse FAQs
How to remove ceiling panels to access cabling on an EcoAisle
Published date:
08 April 2019
Browse FAQs
Issue:
How to remove ceiling panels to access cabling on an EcoAisle.
Product line:
EcoAisle.
Environment:
Only ACRC100, EcoBreeze, ACRC301X..
• Over aisle access
• A customer still needs to access the cabling on top of the racks. This system is designed with the user in mind. Access to the top of the racks is done with out the use of tools. On a ceiling system it is as easy as removing a drop ceiling tile with a lift, angle and drop. The duct system has an air-block system that can be removed with a thumbscrew.