Newly attached camera pod on a version 3 Netbotz appliance does not show time stamp.
Published date:
13 August 2013
Issue:
Newly attached camera pod on a version 3 Netbotz appliance does not show time stamp.
Product Line:
NetBotz version 3 devices
Environment:
NetBotz "botzware" earlier than 3.3
Cause:
Not a default configuration.
Resolution:
The time stamp does not automatically appear on the image on a version 3 Netbotz appliance if a camera pod is added while the appliance is running. The time stamp will appear if the camera pod is attached when the bot is rebooted or if the pod is attached prior to booting the appliance. This happens to both the newer camera pod 160 as well as the older version 2 camera pod 120.
This is addressed in Botzware version 3.3
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.