Browse FAQs

Does the Matrix-UPS charge the batteries in Bypass mode?

Published date: 08 November 2018

The Matrix-UPS does not charge its batteries in bypass mode. It is imperative to get the unit back to an online mode in order to achieve optimal functionality and keep the batteries from discharging over time. Should the Matrix need to be in bypass the battery packs should be disconnected from the Electronics Unit.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.