Serial Communication Cable used for SURTD model UPS models
Published date:
05 March 2018
Issue:
Which serial communication cable can I use with a Smart UPS RT "SURTD" model UPS?
Product Line:
Smart UPS Online models with the following model prefix:
SURTD
Environment:
All serial numbers
All firmware versions
Cause:
Users may need to order a spare communication cable or verify the correct part number.
Resolution:
The SURTD online UPS models use an RJ-45 to DB-9 Serial Cable. The part number is 940-1525A and as a spare part through most resellers or distribution channels using the part number 0J-940-1525A.
This communication cable is shipped with a new UPS.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.