Installing a Smart-UPS in a WX series Netshelter enclosure
Published date:
31 May 2019
Issue:
Installing a Smart-UPS in a WX series Netshelter enclosure
Product Line:
Smart-UPS
Environment:
All rackmount models, All Serial Numbers
Cause:
Product Information
Resolution:
The maximum depth between the rails on a WX series enclosure is 15.5"" and the minimum depth to use the standard Smart-UPS rail kit is 20.75"". In order to mount a standard Smart-UPS in a WX enclosure you must install it in the bottom of the rack without rails. This allows the rear frame of the WX to properly support the Smart-UPS. Secure the front of the Smart-UPS to the front rail of the enclosure using the standard front brackets included with the Smart-UPS.
Please note that the maximum load rating for this rack is 200 lbs, and the maximum equipment depth is 18"", which precludes the use of some larger Smart-UPS models."
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.