Configuring the Windows SNMP Agent for use with PowerChute Business Edition versions 9.2.1 and below
... therefore SNMP Windows service is no longer ... ... click on the Management and Monitoring Tools ... locate Simple Network Management Protocol ... of Simple Network Management Protocol SNMP service will be installed on the system ... ... start automatically after installation . ... to verify the service status from Services in Control Panel ... start the SNMP service from there. Two new services will be created ... SNMP Service which is the ... SNMP Trap Service which receives trap ... messages to SNMP management programs running on ... ... to the SNMP service by default, ... ... Panel-> Administration Tools-> Services ->SNMP service .