Rack PDU 2G (AP8XXX) Network Port Sharing Information
General information regarding the Network ... Capability of AP8XXX Rack PDU models Rack Power Distribution AP8XXX Rack PDU series only ... ability to share one IP address via one network connection) General information ... to the detailed information sections below. ... up to four Rack PDUs using only one ... by connecting the Rack PDUs via the ... ports on the Rack PDU front panel ... All Rack PDUs in the ... using the same Rack PDU firmware revision ... in order to support the Network Port ... ... a number, 1 to 4, ... uniquely identify the Rack PDUs in a ...