Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
... single register in StruxureWare Data Center Expert's modbus output is ... StruxureWare Central / StruxureWare Data center Expert StruxureWare Central any version StruxureWare Data center Expert any version ... single register for StruxureWare is a 16 ... ... as 6553. 5 . ... bit register in StruxureWare . ... this limitation, StruxureWare Data Center Expert can be configured ... StruxureWare does not know ... This is also why this should be done upon initial setup as if the system is already configured and a register is changed, the polling software must be reconfigured with the new registers. ... This math must all done on the side of the querying application .