Browse FAQs



APC UPS Network Management Card (NMC) Compatibility Chart
... Which model of UPS Network Management Card ... supported in my UPS ? UPS Web/SNMP ... UPS Network Management Card ... UPS Network Management Card ... UPS Network Management Card ... ... compatibility between current UPS models and discontinued ... bug fixes will only be available with ... ... use in other UPS systems can be ... UPS Model ... Phase Smart- UPS with the following ... Matrix UPS with UPS firmware versions Y ... Single phase Symmetra models: Symmetra Power Array Symmetra RM 6K ... Symmetra LX Three phase Symmetra models: 20kw Symmetra PX All-In ... 40kw Symmetra PX 80kw Symmetra PX
Symmetra PX1-PX2; What happens when PX1, PX2 and 250/500k PX is EPO'd
... 250/500k PX is EPO'd Symmetra PX ... describes how the Symmetra PX reacts to the ... PX : ... circuit in the Symmetra PX is activated the ... Breaker in the Main Frame or in the XR Frame (80kw units only ) also switches ... Mains feed CB will ... ... output of the XR Battery Frames or on the output of the Symmetra PX UPS . PX : Only the Battery CBs on XR frames will be tripped ... ... input power to UPS . PX : All Battery CBs on battery frames and Q2 will be tripped ... Reset EPO switch and follow proper procedures to restart UPS
What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
This would make for a total of 4 battery frames in addition to the Main UPS frame which houses the Power Modules.
Single Phase Symmetra XR Frame Compatibility
Issue Single Phase Symmetra XR frames are compatible only with certain UPS systems.
Mounting the Symmetra LX in a 2 post rack
Symmetra LX ships with ... post rail kit only , however it ... safely mount the UPS system and any associated XR frames in a 2 post ...
Treck TCP/IP Vulnerabilities (ripple20)
Release notes Network Management Card 2 for Symmetra PX 48/96/100/ 160 kW UPS
E3 error message on the Symmetra Extended Run Battery Frame (XR frame)
The XR frame of a single phase Symmetra displays E3 ... mainframe indicates an XR Frame Fault. Symmetra Power Array Symmetra RM Symmetra LX ... message on the Symmetra XR Frame is an ... communication between the Symmetra mainframe and the Symmetra Extended Run ( XR ) Battery Frame ... ... between the two frames where the Power ... located in the XR Frame. ... a communication issue only , and in ... function of the UPS if it were ... ... that event the UPS goes on battery ... ... card on the Symmetra Extended Run Frame ... ... back of the Symmetra Extended Run Battery ...
Batteries discharged to a low voltage in a single phase Symmetra frame
Single phase Symmetra battery modules are ... the system will only be able to ... Symmetra Power Array Symmetra RM Symmetra LX ... , it is important that this fault ... ... happens, the only way to provide ... to place the UPS into a bypass ... ... installed in a Symmetra frame, it ... If the Symmetra is powered down ... ... happens, the only way to provide ... to place the UPS into a bypass ... All Symmetra and Symmetra RM units ship ... : Symmetra LX was designed ... ... This specific cause only applies to Symmetra Power Array and Symmetra RM. The Symmetra will not be ...
AOS v6.3.2/sy3p APP v6.3.2 UPS Network Management Card 2 (NMC2) ap9630/AP9631 UPS Compatibility
... the compatibility of UPS Network Management Card ... UPS Network Management Card ... ... Facility 3 Phase UPS - Symmetra PX ... Facility 3 Phase UPS product catalog, ... different varities of Symmetra PX including 20, ... 100, and 160 kVA models. ... Management Card compatibility Symmetra PX (if needed ... ... provide support for Symmetra PX 20, 40 ... 80 kVA models only (especially to ... ... has historically supported Symmetra PX 20, 40 ... as well as Symmetra PX 48, 96 ... 100, and 160 kVA models with ... ... to monitor their UPS only .
Serial communications between Smart-UPS VTs, Galaxy 3500, and Symmetra PX with IBM AS/400, i Series
If the NMC is needed and your UPS only has one SmartSlot ... serial port of the UPS and install the NMC in the chassis.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.