Browse FAQs



What are the various generations of Smart-UPS Products?
... of single phase Smart-UPS Products? Smart-UPS ... a variety of Smart-UPS products in use ... ... Over the years APC has steadily improved ... ... refer to the apc .com product ... for your specific UPS . Current Products: ... generation Line Interactive Smart-UPS products 750va - 3kva Fully interactive LCD display ... -45 Serial Port on UPS ) Smart -Slot for installation of APC Accessory Cards ... generation Line Interactive Smart-UPS products 750va - 3kva Fully interactive LCD display All units Rack / Tower convertible ... -45 Serial Port on UPS )
Smart-UPS C Series FAQ
Smart-UPS C Series FAQ Smart-UPS ... is the new Smart-UPS C series? The Smart-UPS C series is ... new entry level Smart-UPS product designed for ... ... feature a new LCD Interface. ... dedicated Tower or Rack - Mount models in 1000 ... ... 1500va in both Rack and Tower form ... ... with the SMC Smart-UPS ? The SMC Smart-UPS supports Powerchute Business ... ... not have a Smart -Slot and ... ... smc1500c) include Smartconnect Cloud Connectivity What communications ports are available?
Installing Standard APC Rails to a Threaded Rack
Smart-UPS , rack mount , rails, threaded, rack
Frequently Asked Questions for the new SMX and SMT series of Smart-UPS products.
... SMT series of Smart-UPS products. Smart-UPS SMT and SMX ... SMX series of Smart-UPS is an all new generation of Smart-UPS product with many ... UPS Frequently Asked Questions ... November 2009 new Smart - New Smart -models are ... by their intuitive LCD interface. APC’s patent pending ‘ ... ... do the new UPS’s not have a DB9 serial port ? ... RJ45 style serial port in addition to a USB port and both cables ... ... DB9 style serial port was not used ... New Smart-UPS models utilize PowerChute ...
Is there a NetShelter Accessory Compatibility Chart that shows which NetShelter accessories, UPS, PDU, Symmetra, NetBotz, Air or KVM fit into a specific cabinet?
... also includes other APC /SE product families that can mount into a NetShelter ... , such as Smart-UPS , rPDUs, NetBotz, Rack Air and KVMs ...
How to assign a fixed IP address to SmartConnect enabled Smart-UPS
... like it configure SmartConnect enabled Smart-UPS with a fixed ... ... SMC, model Smart-UPS with embedded SmartConnect network port . Smart-UPS with embedded SmartConnect network port ... and SMTL model Smart-UPS From the LCD panel scroll to ... ... arrow scroll to UPS IP Address Settings ... From the UPS IP Address Setting ... ... any SMT model Smart-UPS with firmware less ... ... for the embedded SmartConnect network port you must log ... the router the UPS is connected to ... ... address of the UPS that has registered ... The mac address is the product ID number found on the sticker on top of the UPS .
Video: How to mount a Rack Mount Symmetra or Rack Mount Smart-UPS to a 2 Post Rack?
Issue: Mounting a Rack Mount Symmetra or Rack Mount Smart-UPS to a 2 Post Rack
What are the Minimum and Maximum mounting depths for Smart-UPS rails?
... Minimum and Maximum mounting depths for Smart-UPS rack mount rails? Smart-UPS All rack mounted models, All ... ... This includes the UPS as well as ... Smart-UPS Rackmount units ( ... and brackets to mount the unit in a typical IT rack enclosure. ... of different sized racks . ... of how to mount your unit, ... included with your UPS or External Battery ... For all Smart-UPS products 10kva or ... If your Smart-UPS is equipped with ... sides of the Smart-UPS chassis that slide ... For Smart-UPS products over than ...
How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SLC/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: ... firmware of the UPS : All Smart-UPS ... support the below Smart-UPS devices: ... smx1500 with firmware UPS 02.x ... ... find your current UPS Firmware version via UPS LCD : ... menu of the UPS LCD screen , select " ... down to " UPS Firmware". ... find your current UPS Firmware version via ... ... find your current UPS ID: Every Smart-UPS has a unique UPS ID. ... menu on the UPS LCD screen , or via ... ... same models of UPS have different UPS IDs depending on ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.