PowerChute Network Shutdown 4.3 fails to power off VMware ESXi 6.7 U3 host
Published date:
23 March 2020
Issue:
PowerChute Network Shutdown 4.3 fails to power off VMware ESXi 6.7 U3 host with error
ERROR Thread-82 com.apcc.m11.components.Shutdowner.Hosts.ESXUnmanagedStandaloneHost com.vmware.vim25.RestrictedVersion: Current license or ESXi version prohibits execution of the requested operation.
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method) - hostShutdown
Product Line:
PowerChute Network Shutdown v4.3
Environment:
VMware ESXi 6.7 U3 host with VMware vSphere 6 Essentials Plus license.
Cause:
Change to VMware ESXi 6.7 License
Solution:
User must contact VMware for assistance with the licensing.
Per VMware knowledge base document 1023990 vSphere Essential Plus license should allow CLI access to the host.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.