Galaxy VS; Why is FTP being logged in the event log but no external cause for logging FTP found?
Published date:
25 February 2020
Issue: FTP is being logged in the event log but no external cause for logging FTP
Product line: Galaxy VS
Environment: Galaxy VS
Cause: Bug in the current firmware 4.28. Some UPS to NMC communications like Waveform generation are being logged by the NMC. FTP events should be communications between NMC and external applications such as EcoStruXure IT or DCE.
Resolution: Next firmware release should resolve this logging anomaly.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.