What size are the cable ports on the NetShelter CX, and how many are there?
Published date:
28 August 2019
Issue:
Cables need to enter and exit the cabinet.
Product Line:
NetShelter CX2
Environment: All versions and serial ranges.
Cause:
Knowing the dimension of the cable port allows a person to calculate how many cables can fit through the opening.
Resolution:
AR4000MV: two ports, 30mm x 95mm at the botton and 26mm x 68mm at the top. AR4018A/AR4018IA: one port, 350mm x 120mm at the bottom. AR4024A/AR4024IA: one port, 350mm x 120mm at the bottom.
AR4038A/AR4038IA: two ports, 350mm x 120mm, one at the top and one at the bottom.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.