How many leak sensor cables can be attached in series on any 300 mm units.
Published date:
14 July 2020
Issue:
This document answers the question on how many leak sensor cables can be attached in series on any 300 mm units.
Product line:
All 300 mm units
Environment:
All Serials.
Cause:
Install.
Resolution:
Leak detector port Rope water detector (AP9325). Up to four optional rope water detectors can be installed in series. The rope water detector connects to the RJ45 leak detector port located at the top of the interface box.