Browse FAQs

What is the Frequency Range for Network FM fan blowers

Published date: 06 November 2018




Issue:
What is the Frequency Range for Network FM fan blowers.                                                 

Product line:
Network Air FM CRAC Units. 

Environment:
Data Center Room coolers. 

Cause:
Informational the settings below are recommended settings for each size model unit.

Resolution:

FM35 - 35hz

FM40 - 40hz

FM50 – 48-52 hz

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.