How do I select the correct Smart-UPS XL battery pack for my Legacy Smart-UPS?
Published date:
05 June 2019
Issue:
How do I select the correct Smart-UPS XL battery pack for my Legacy Smart-UPS?
Product Line:
Smart-UPS
Environment:
SU and SUA "XL" models, All Serial Numbers
Cause:
"XL" models allow for the use of external batteries to extend runtime.
Resolution:
"APC manufactures a wide VA range of Smart-UPS products. Some of these models
have large, more robust battery chargers. This allows the user to add
additional external battery packs to the Smart-UPS. This feature increases the
runtime when operating on battery. It is important to understand which
Smart-UPS will function with the appropriate external battery pack.
*All Smart-UPS with the extended run feature, will have the letters ""XL"" in the part number. The only exceptions would include the SU3000NET, SU3000TNET and the SU3000RMNET.
The chart below contains all current production Smart-UPS, as well as recently
discontinued Smart-UPS, which support an additional battery pack, and the battery
packs with which they are compatible.
UPS Model
Battery Pack Model
SU700XLNET (disc.)
SU24XLBP or UXBP24
SUA750XL
SUA24XLBP (will work w/ SU24XLBP and UXBP24, but they are different colors)
SU1000XLNET (disc.)
SU24XLBP or UXBP24
SUA1000XL
SUA24XLBP (will work w/ SU24XLBP and UXBP24, but they are different colors)
SU2200XLNET
SU48XLBP or UXBP48
SU1400RMXL3U
SU24RMXLBP2U only
SU1400RMXLNET (disc.)
SU48RMXLBP or UXBP48 (not rack-mountable)
SU2200RMXLNET (disc.)
SU48RMXLBP or UXBP48 (not rack-mountable)
SU2200RMXL3U
SU48RMXLBP3U only
SU3000RMXL3U
SU48RMXLBP3U only
SU2200XLTNET
SU48XLBP or UXBP48
SU2200RMXLTNET
SU48RMXLBP or UXBP48 (not rack-mountable)
SU3000NET
SU48BP only
SU3000TNET
SU48BP only
SU3000RMNET
SU48BP only (not rack-mountable)
SU5000RMXLT5U
SU48R3XLBP only
"
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.