Browse FAQs



What solution does APC recommend for protecting a VDSL data-line?
... line surge suppression for VDSL networks, either of these two models should be recommended, depending whether the application requires rack -mount or ...
AP8XXX Rack PDU 2G "NMC CAN Bus Off" Error
After a "CAN bus off" alarm has been resolved , the clearing event is not generated and the alarm remains in the active ...
v6.X.X Network Management Card 2 "Reset All" or "Reset to Defaults" Command Does Not Work
... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/Switched Rack PDUs (AP86XX ... ... In order to resolve the issue, ... 2 .) Manually delete the required database to reset the settings. ... Type cd db Type delete cfg2.db ... To also remove the current TCP/IP settings, type delete net.db Type reboot ... Type cd db Type del cfg2.db ... To also remove the current TCP/IP settings, type del net.db Type bye ... This step can be done one of two ways:
Why is my Web/SNMP (ap9606) or Network Management Card 1, 2 or 3 not recognizing my UPS or device?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Network Management Card 2 (NMC2) ... Devices with an embedded Network Management Card 2 include (but are not limited to): 2 G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products. ... Device Type ... Rack Power Distribution Units Rack Power Distribution APP or rpdu ... Lastly, if the firmware upgrade does not resolve the issue, there may be a problem with the Network Management Card or the UPS SmartSlot.
Network Management Card 2 Firmware v6.X.X FAQ/Upgrade Issues
... Network Management Card 2 (NMC2) ... ... Network Management Card 2 upgrade from v ... ... Network Management Card 2 - ap9630/ ... ... Network Management Card 2 include (but ... to): 2 G Metered/Switched Rack PDUs (AP84XX ... ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 upgrade from v ... ... Network Management Card 2 "Reset All ... ... Network Management Card 2 config.ini ... Network Management Card 2 config.ini ... ... Network Management Card 2 (NMC2) ... .X User Types and Permissions Definitions ... Network Management Card 2 (NMC2) ...
Are there any NetShelter products or solutions certified by Cisco?
... APC's products or solutions that are Cisco ... ... certain products or solutions to work with ... ... the Schneider Electric solutions for Cisco are ... Developer Network Marketplace Solutions Catalog: ... =%E 2 %9C ... ... title of a solution it will open ... The specific solutions for NetShelter are ... - Rack Power Distribution with ... Any solution with the “ ... ... all" for solutions . ... example of a solution that is not ... certified is the solution for Catalyst and ... ... had a released solution to the market ... ... a "certified solution ".
Why are the red outlet LEDs always scrolling on Rack PDU models AP7855 or AP7867?
AP78XX Metered Rack PDU models, specifically ... There are two scenarios that can lead to this condition: ... Manually changing these values or resetting the unit to default settings should resolve this issue. Scenario 2 : ... There are two ways to calibrate the unit with help of these menus: ... Connect a known load (must be greater than 5A) on L1 Outlet 2 . Then select the fourth menu "Calibrate the unit". ... If the user does not have the ability to connect a known load on L1 outlet 2 then follow this second procedure.
Network Management Card 2 (NMC2) - snmpv1/v3 walk beginning at .iso through .iso.org.dod.internet does not work properly
... Network Management Card 2 device. ... generic mib- 2 OIDs are returned ... Network Management Card 2 - ap9630/ap9630ch, AP9631/AP9631CH, AP9635/35CH Devices with an embedded Network Management Card 2 include (but are not limited to): 2 G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products. ... This issue is resolved in AOS 6.1.2 or higher.
Network Management Card 2 config.ini upload for event notification settings does not enable events in v6.X.X
As noted in (Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) ... Network Management Card 2 - ap9630/30ch, AP9631/31CH, AP9635/35CH Devices with an embedded Network Management Card 2 include (but are not limited to): 2 G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products. ... This issue is resolved in a future version of firmware, AOSv 6.1.1 or higher.
Domain Name/DNS Hostname Parameters on the Network Management Card 1 and 2
... Card 1 and 2 ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Network Management Card 2 - ap9630/ ... ... Network Management Card 2 include (but ... to): 2 G Metered/Switched Rack PDUs (AP84XX ... resolves this issue. ... Network Management Card 2 Behavior For the Network Management Card 2 (ap9630, AP9631, AP9635), or any device with an embedded card, leading numbers in domain names are not accepted in the DNS hostname field in v5.X.X firmware, This has been ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.