Browse FAQs



Does installing a 3rd party accessory onto a NetShelter cabinet impact the cabinet's warranty?
Cause: When planning to install a 3rd party accessory onto a NetShelter cabinet.
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
IF you plan to install a Rack Expansion Bundle Kit next ... acdc1008, not included) must be installed on the PDU or UPS.
Single Phase Symmetra Extended Run (XR) Frame Cable Lengths
This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example.
What are the Dynamic Load ratings and Shipping Load ratings for NetShelter CX cabinets?
Persons planning data centers need ... CX for static installation , dynamic installation (rolling on flat surface) or to ship loaded with equipment.
Data Center Expert | Starting with a fresh install
If you plan to re-import a previous backup, be sure that you have not only made a backup but that you also ...
Steps to take when moving a Symmetra Power Array from one location to another
... Manual" (Chapter 3, "Unpacking and Installing Frame) to ... or if you plan on moving your UPS in the future.
How does the EcoAisle accommodate lighting without interfering with the ceiling panels.
Install ... • Many datacenters are planned around the floor tiles, but planning also needs to happen for the illumination of the aisles between the rows of racks. ... Installation of the light kits and wire routing is integrated into the extrusion of the ceiling panel support rails
Problem: PowerChute Network Shutdown does not turn off the UPS following a shutdown event.
Because of this 100-second interval, PowerChute might not have received this information in a couple of situations: a) immediately after installing PowerChute or b) after a restart of the PowerChute service, e.g. after a reboot. To make sure the UPS turns off as planned when a shutdown event occurs, PowerChute shutdown events should be configured with a delay of 120 seconds.
Can the ACRC, ACRD, ACRP, or ACSC be grouped together?
Install , Repair ... There has been some discussion about supporting heterogeneous groups for the In Row products, but currently there are no approved plans at the moment.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.