Browse FAQs



APC UPS Network Management Card (NMC) Compatibility Chart
... Which model of UPS Network Management Card is supported in my UPS ? UPS Network Management Card 3 - ... PS Network Management Card 4 - ... UPS Network Management Card 2 - ... UPS Network Management Card 1 - ... UPS Web/SNMP ... ... /en/ tools /download/ ... Some of these management cards are older ... ... compatibility between current UPS models and discontinued management cards, support ... device features or management card features and bug fixes will only be available with ... generation of Network Management Card for your ... ... Current generation Network Management Cards purchased on ... the Smart- UPS family.
Chinese language does not work properly with sumx & sy UPS Network Management Card 2 (NMC2) applications v6.2.1
... language option for UPS Network Management Card 2 sumx ... UPS Network Management Card 2 - ... ... for Smart- UPS and Symmetra single phase UPS models) ... new Chinese- only language pack has ... The .lpk language pack files are available for download at apc.com (https://www.apc.com/ tools /download/index.cfm) and attached to this knowledge base for your convenience. ... This replacement Chinese- only pack will need to be uploaded/changed by FTP or SCP rather than during a firmware upgrade.
Why can't I use an international model SU, SUA, SUM, SMT, or SMX series Smart-UPS in North American 208v or 120v environments?
... series Smart- UPS in North American ... Smart- UPS ... All Smart- UPS international models can ... ... 230v Smart- UPS units would not ... ... to Ground( H -G) ... There is, however, full surge suppression between Hot and Neutral ( H -N). ... International Model Smart- UPS can be identified in several ways: The box in which it is shipped has a sticker on the outside that indicates 220-240vac, International Use Only .
PowerChute Network Shutdown 2.2.4 and 4.5G and 5G Smart UPS Behavior
... 4 and Network Management Card 2 UPS application firmware revision ... turn off the UPS via PowerChute Network ... is supported for only the 'On ... Low Battery' UPS events on certain Smart- UPS models. ... the turn off UPS functionality via PowerChute ... events, the UPS will not turn ... Smart- UPS Models: UPS Network Management Card 2 ... application for particular UPS models. ... .com/ tools /download. ... turn off the UPS and then turn ... Any prior version of PowerChute Network Shutdown will not work with the aforementioned UPS models.
PowerChute Network Shutdown lost communications or cannot establish communication with UPS.
... establish communication with UPS . ... type of Network Management Card being used ... The Network Management Cards that are ... and AP9641 are only compatible with PCNS ... ... with the network management card during installation ... ... that there is only one install daemon ... ... and above can only run 1 instance ... ... Check the Network Management Card to see ... ... that the Network Management Card and the ... ... with the Network Management Card when the ... ... connected to one UPS ) ... on the Network Management Card has not ... This option can be found under the System> Tools menu on the Network Management Card for AP9617, AP9618, AP9619.
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
... to Smart- UPS drops or reboots ... Smart- UPS ... a Smart- UPS can be dropped ... - A UPS with a weak ... ... Every Smart- UPS has a " ... ... ), will only be good for ... ... failure which the UPS self test may ... ... result in unexpected UPS behavior including load drops and the UPS turning off: - Each UPS is limited in ... ... number of the UPS tells you the ... ... determine if your UPS is capable of ... please use our UPS Selector Tool at ... plugged into the UPS , but the ... . If the UPS and surge strip ...
How to download and use the APC UPS-Link Protocol Language
... to obtain APC UPS -Link Protocol ... Smart- UPS , Matrix, ... The UPS -Link Protocol is used only for APC smart signaling UPS models. This UPS -Link Protocol ... ... other next generation UPS's without the use ... ... now download the UPS -Link language ... ... on the contract only . ... .com/ tools /download/ ... ... To download the UPS -Link Protocol ... ... before downloading the UPS -Link Protocol ... Standard UPS -Link Protocol ... UPS -Link License ... for APC AV UPS's (e. ... Once downloaded, users can use the UPS -Link protocol freely within the conditions of the Licensing Agreement.
Why might the LEDs on my Back-UPS or Smart-UPS SC be flashing?
... and Smart- UPS SC: causes ... ... , Smart- UPS SC 620va and ... ... indicates that the UPS is performing a ... ... indicates that the UPS has entered " ... " where the UPS will turn off ... The UPS is put into ... ... Guide) your ups may "" ... ... "" your UPS , press the ... ... indicates that the UPS is operating normally ... ... indicates that your UPS is operating on ... The UPS can only provide power from ... If your UPS is operating on ... ... mind that the UPS will run on battery whenever UPS deems the power ... APC UPS Selector tool
Video: How to Select the Correct Replacement Battery Cartridge (RBC) for your UPS
The UPS indicates battery replacement ... to when the UPS was first put ... Smart- UPS and Back- ... ... maintenance for your UPS . UPS Replacement Battery Selector ... for your APC UPS and to see ... tool on www. ... ... you use this tool , you will ... to know your UPS model #. ... To find your UPS model #, ... sticker on your UPS . ... bottom of your UPS . ... sticker indicates the UPS model number. ... row indicates the UPS serial number. ... year that the UPS was manufactured. ... age of the UPS will also help ...
AOS v6.3.2/sy3p APP v6.3.2 UPS Network Management Card 2 (NMC2) ap9630/AP9631 UPS Compatibility
ap9630/31 SmartSlot card, which users can add to their system to monitor their UPS only .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.