Browse FAQs

How does the modulation of the electric heaters work on an ACRP unit?

Published date: 17 July 2020

Issue:  
How does the modulation of the electric heaters work on an ACRP unit?

Product line:
ACRP1XX, ACRP5XX.

Environment:  
All Serial Numbers.

Cause:  
Install, Repair.

Resolution:
Each heater is turned on as needed so the CW unit has three stages: 33.33%, 66.66%, and 100%. The DX unit has two stages: 50% and 100%.
 
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.