Browse FAQs

Details Returned from NetBotz Devices via Advanced Device Crawlers

Published date: 17 July 2020

Issue:

Details Returned from NetBotz Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for NetBotz appliances assuming the NetBotz DDF (Device Definition File) is installed on the server appliance and the client appliance is SNMP enabled. Please note that not all information listed below is available on all NetBotz models.

Resolution:

 
  • Model
  • Temperature
  • Humidity
  • Airflow
  • Audio Alarm
  • Door Switch
  • Camera Motion

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.