Browse FAQs

Details Returned from Juniper Devices via Advanced Device Crawlers

Published date: 17 July 2020

Issue:

Details Returned from Juniper Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Juniper systems assuming the Juniper DDF (Device Definition File) is installed on the NetBotz appliance and the Juniper system is SNMP enabled. Please note that not all information listed below is available on all Juniper models.

Resolution:

.
 
  • Description
  • Temperature
  • Redundancy Switchover Count
  • Redundancy Switchover Time
  • Switchover Reason
  • Redundancy Keepalive Heartbeat Period(0
  • Redundancy Keepalive Timeout before Transferring to Backup
  • Redundancy Time Elapsed since Receiving Keepalive Message
  • Redundancy Keepalive Losses

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.