FAQs durchsuchen



Assigning global permission for newly created user is not allowed in vSphere vCenter 6.0 U 1b and 6.0 U 2a.
vCenter cluster having more than two nodes . vCenter Server is installed on ... ... your windows vCenter Server ... c:\ Program Files\MIT ... Copy the path (eg: c:\ Program Files\MIT\Kerberos\bin) Navigate to the registry path: HKEY_USERS\S- 1 -5-18\Environment ... eg: C:\ Program Files\*******; c:\ Program Files\MIT\Kerberos\bin ... Restart the Windows vCenter server
Creating an Aggregate Device within the KVM Access Software
... KVM Access Management Software and why it ... KVM Access Software (ships with ... ... wishing to consolidate nodes within their KVM Access Software All software versions ... (router, server , ethernet switch ... ... ports into a single Aggregate Device, ... counts as a single node , and only requires a single license. ... to that specific server without having to ... ... through the Access Software . When a ... down a specific server remotely they don't ... ... I have 300 node license but have 300 servers and 600 PDU ... devices, ( servers and PDU ports ...
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
1 . In a ... ... add a new server , please click ... ... against an existing server please jump to ... ... = StruxureWare Data Center Expert Basic ... = StruxureWare Data Center Expert Standard ... = StruxureWare Data Center Expert Enterprise ... = StruxureWare Data Center Expert Virtual Machine ... = StruxureWare Data Center Operation ... a hardware DCE server and in help ... VM or Data Center Operation . ... verify that the node count is correct ... ... a word processing application such as notepad ... 12. Select System -> Server Administration Settings -> License Keys ... 14. Paste the license key(s) one at a time into the popup box.
Data Center Expert | How do hardware and software support contracts work?
... hardware warranty and software support contracts work for StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Software Support Contract StruxureWare Data Center Expert appliances come ... software support. The Data Center Expert appliance and ... active and complete software support in order ... technical support and software upgrades. Software support contracts are required for the server which has a default 25 nodes (covered under base software support SKUs) ... as each additional node license. StruxureWare Data Center Expert Appliances can ... Year 1 Software Support Contracts Software support can not ...
Video: Data Center Operation | How to create logs if httpd service is down?
1 . Log into the Operation server via console or SSH. 2. Enter "cd /"
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
... the StruxureWare Data Center Operation StruxureWare Data Center Operation StruxureWare Data Center Operation (All Versions ... ... that the Apache server (httpd ... files from the server in this state ... ... " from the Operation server using SFTP/ ... In this document, we will be using a free program called WinSCP. You can find this program . Please see the instructions below for a step by step guide for "downloading" files from the server via WinSCP. 1 . Open the application ... 1 . Double click on data folder ... 3. Locate the backup to save off server ... 1 . Double click on /tmp folder
Data Center Operation | Server is running low of storage space.
StruxureWare Data Center Operation , DCO, Purge, data, Application crash, hard disk, storage
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... base . Note that if your previous server already has licensing on it (beyond the base 25 device nodes and 1 surveillance node ) ...
How to deploy PowerChute Network Shutdown v4.3, v4.4 Appliance in vSAN cluster.
... of the vSAN Cluster . PowerChute Network Shutdown Appliance version v4.3, v4.4 deployed on vSAN Datastore on one of the Hosts that is part of the vSAN Cluster . ... Software issue ... Server = 192.168. 1 .190 Server _Protocol = https Server _PORT = 443 ... We will only support Single /Redundant UPS Configurations. For vSAN Stretched Cluster , PCNS needs to be deployed on the Management Host (runs the Witness Appliance outside the vSAN Cluster ).
Data Center Expert | What virtualization environments are supported?
The Data Center Expert v7.x server is available as a virtual appliance, supported on VMware ESXi 6.5.0. The full-featured demo of the virtual appliance monitors up to five device nodes and one surveillance node . You can purchase a license key to upgrade to a production version to monitor additional device nodes and activate supported applications , or to migrate from a server hardware version to a virtual appliance.


Ergebnisse 1 - 10 von 64

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.