FAQs durchsuchen



Technical Spec’s on a acpa4000
... 60% 8257 kW Kw ... Power Consumption ( kW ) 1.6 kw /hr is ... Plug CFG NEMA 5 -20 Min ... Voltage 110- 120 typical is 3.8a Air Differential switch Factory setting . 8 ... restart to prevent damage Automatic Restart Yes If power is cut unit will return to last known operating condition upon power up Programmable Thermostat Yes Control Panel Yes Programmable Schedules Yes Key Features ... Operating Cost per hour ($.14/ kW ) $
Uniflair Manual Start Up and Shut Down (PCO1)
Uniflair Manual Start Up and Shut Down (PCO1) ... Start Up the Unit ... 5 . Install the cover metal sheet to the electrical panel and secure with the screws. ... 8 . Close the door and the front panels. ... 1. On the first user interface screen, press the UP or DOWN buttons until the SWITCH OFF UNIT screen appears.
How to enable .NET 2.0 on Windows 8.x and 10
PowerChute Personal Edition 3.0.2 will not install on Windows 8 or 10 because the system in missing .Net ... Windows 8 .x and 10 ... 1. Open up the control panel. (Right click start - then click control panel) ... 5 . You should see .NET Framework 3.5 (includes .NET
SRT 8 or 10kva reports Error P.11 or DC Bus Soft Start or event codes 124/125
4. Improved system handling for certain AC input conditions during system start - up .
SRT 8 or 10kva experiences excessive battery transfer and re-transfer events in 3 phase systems
4. Improved system handling for certain AC input conditions during system start - up .
SRT 8 or 10kva reports Error P.11 or DC Bus Voltage Low or event codes 128/129
4. Improved system handling for certain AC input conditions during system start - up .
Video: Data Center Expert | Backing up to a Windows Share
5 ) Set the ... 8 ) Ensure that ... ... user as step 5 ). 10 ) Set the ... ... Steps 3 & 5 ) 5 ) Select Test Mount. ... 7) Select the backup in the list and then select Start Backup. ... The OS upgrade will allow for the implementation of support for higher version of SMB. We do not currently have a time-frame available for completition for implementation of higher levels of SMB support as the OS upgrade needs to be completed first . ... This can cause Data Center Expert to be unable to back up to existing shares or mount new shares.
How to replace an actuator on a Network Air FM unit
Valve actuator service ... 2. Loosen the two 10 mm nuts securing the actuator to the valve shaft. ... 4. Pull the actuator up and off the shaft. ... 5 . Reverse this procedure to install the new actuator. ... To access the MultiCool/Economizer valve actuator, first remove the condenser fluid valve actuator and the actuator shaft bracket. 1. Use an 8 mm wrench to remove the three bolts that secure the
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... device from v 5 .X. ... ... /AP9617/ 8 /9 installed ... AP9631 use version 5 .X or ... ... device from v 5 .X. ... 5 . Add the ... 8 . Wait for 2- 5 minutes for the ... ... as long as 5 -7 minutes ... ... will need to first upgrade to AOS ... ... then stop that service . ... no parity, 8 data bits, ... 5 . Enter the ... 6. Start an XMODEM transfer ... 8 . Select option ... 10 . Select option ... ... box that pops up , browse the ... ... should be transferred first and then the ...
DAC, Cancoil Installation Manual
... ….. 5 ... ….. 5 Section 5 . Start Up and Check Out ... ….. 5 ... and set- up are required for ... ... unit for proper servicing and preventative maintenance ... ... will return oil up a vertical riser ... ... ” drop per 10 feet of length ... ... assure oil flow up to the condenser ... ... charge (page 8 ) plus the ... ... ” drop per 10 feet of length ... ... All hook- up , evacuation, ... - Before starting the unit, ... Section 5 . Start - up and Check Out ... ... must be within 10 % of the ...


Ergebnisse 1 - 10 von 82

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.