FAQs durchsuchen



Refrigerant charging table for a Uniflair Unit
... table for a Uniflair Unit. ... Air-cooled DX units must be ... Systems with remote outdoor condensers ... ... lines in accordance with applicable industry guidelines ... ... refrigerant lines/ chilled water piping are free from debris. ... 8 BCuP- 5 . ... pipes are installed with proper supports and ... ... lines is between 5 m/s ... discharge lines are up to 68.9 kPa ( 10 psi). ... a minimum of 10 mm per m ... ... pre-charged with nitrogen. 1 . Open any ... ... 250 psi) with nitrogen. 1 . Open any ...
Uniflair Manual Start Up and Shut Down (PCO1)
Uniflair Manual Start Up and Shut Down ... Start Up the Unit 1 . Unlock the ... 5 . Install the ... panel and secure with the screws. ... pre-charged with water and all ... 8 . Close the door and the front panels. ... If an alarm is indicated, consult the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual. ... 1 . On the first user interface screen, press the UP or DOWN buttons until the SWITCH OFF UNIT screen appears. ... For additional information, see the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual.
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS ... ... in for assistance with Powering Down the ... ... is for a single UPS with an external maintenance ... ... mount, or free standing, the ... Step 1 : Touch any button on the display to wake it up . ... Step 5 : Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch. ... Step 8 : Unlock CB2, remove the key, and place it in the key interlock. ... Step 10 : Turn off the CB3 Input Breaker ... Turn off Q 1 Switch
DAC, Cancoil Installation Manual
Section 1 . Warranty and ... ... ….. 5 ... ….. 5 Section 5 . Start Up and Check Out ... ….. 5 Section 1 . As with all refrigeration equipment ... and set- up are required for ... ... file a claim with the shipping company ... ... place a claim with the shipping company ... ... under the chassis with a forklift or with a spreader bar ... ... contractor in accordance with applicable codes and ... ... and dry and free of all debris ... ... purge the system with dry nitrogen during ... ... are based on 1 degree per 100 ... ... will return oil up a vertical riser ...
APC Schneider Cooling Unit Identification
... coil C= Chilled Water C= Chilled Water ... Main C= Chilled Water ... AFX 018 ( 5 T) 27 ( 8 T) AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) 10 (2 Bay ... ... CM 003 ( 1 T) 017 ( 5 T) A ... C= Chilled Water BC= ... -230/ 1 /60 ... =277/ 1 /60 1 - 5 T Air Cooled ... 1 -3T ... 4- 5 T Ducted Only C= Chilled Water
How do I go about Resetting or Reconfiguring my DG5 board.
4. Use the Up or Down arrow to select your model. a. Models Available: CCT- DX , CCT-CW, CG, Versacool, AFX- 1 , AFX-2, Ceiling Mount- DX , Ceiling Mount-CW, Techcool- DX , Techcool-CW 5 . Press the enter after selecting the correct model 6. When you see the Digital Inputs page scroll down with the down arrow as fast as possible. ... 8 . Turn the unit back on after waiting 5 seconds.
Treck TCP/IP Vulnerabilities (ripple20)
To stay up to date on ... ... pre-installed with Smart-UPS ... Devices with an embedded Network ... ... specific CVE associated with the issues are ... ... -UPS, 1 -Phase Symmetra ... and Galaxy 3500 with Network Management Card ... SY ( Single Phase Symmetra) SY ( Single Phase Symmetra) ... 150 kVA PDU with 84 Poles ( ... PDPM72F- 5 U, PDPM138H- 5 U, PDPM144F ... ... Switched Rack PDUs with embedded NMC2 ... Environmental Monitoring Unit with embedded NMC2 Uniflair LE Perimeter Cooling ... Uniflair LE DX Perimeter Cooling Display ... Uniflair LEL Perimeter Cooling ... Uniflair DSA Trim Chiller ...
Video: How to set up load assist on a Uniflair unit.
How to set up load assist on a Uniflair unit. ... Uniflair Gen 1 and Chilled Water Units. ... Uniflair units with push button displays and all Uniflair Chilled Water Units. ... These are the instructions on how to set up a Uniflair unit to turn on for load assist. Load assist in a Uniflair united is referred to as Sleep Mode. ... This operation will only work with two or more units and they must be grouped together.
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
1 ) You must ... to activate the free AP94VMTRL trial virtual ... ... deploy the AP94VMTRL free DCE trial VM ... ... device nodes and 1 surveillance node) ... ... support will work with the contract administrators ... 5 ) During deployment ... ... the first boot up of the DCE ... 6) Back up your hardware server. ... 8 ) Boot the VM and import the backup you've just created from the hardware server. 9) Import the license keys (starting with the VM activation key) created from the previous registration step.
Video: How to change Humidify and Dehumidify set points in a Uniflair unit.
Product line: All Gen 1 Uniflairs with push button displays and all Chilled Water Uniflairs


Ergebnisse 1 - 10 von 69

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.