FAQs durchsuchen



How are the vertical mounting rails oriented (left / right) in the NetShelter cabinets?
Issue: When purchasing a replacement vertical mounting rail it's important to know the difference between a Left Hand rail and a Right Hand rail.
Is there a quick fix for stuck screws on the vertical mounting rails of a NetShelter cabinet?
Issue: The screws on the vertical mounting rail will not loosen.
Do the 800 mm wide NetShelter SV cabinets have 1U rackmount spaces in the vertical mounting rails?
Cause: It appears there may be a 1U punch out in the vertical mounting rails.
What's the vertical mounting rail depth for the NetShelter SX cabinets?
Vertical mounting rails come factory installed on most NetShelter SX cabinets in the proper position for use with rack mountable equipment that has a depth ...
When finger-style vertical cable managers are used in a 750mm wide NetShelter cabinet, is it possible to also block off the cable pass-thru openings in the mounting rails?
It's a brush strip style airflow management product that allows cables to pass through. It installs onto the vertical mounting rail.
Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
... a 2-piece item, and both pieces are required to fully populate one vertical mounting rail in the cabinet.
Can the NetShelter AV busbar be installed into other NetShelter cabinets?
Resolution: The AR8395 can be installed into any NetShelter cabinet that has 20u vertical mounting space available.
Is it possible to convert a NetShelter SX Networking cabinet into a standard NetShelter SX cabinet?
Remove all four existing vertical mounting rails, including the finger-style cable managers in the front and the mounting flange on the left ...
Why are the Dell ReadyRails II loose?
The ReadyRails have a square feature that will seat firmly into the square hole in the NetShelter's vertical mounting rail.
Can the AR8125 NetShelter AV Sliding Shelf be installed into an SX cabinet?
With additional hardware the AR8125 can be mounted into an SX cabinet, or any cabinet with square hole vertical mounting rails.


Ergebnisse 1 - 10 von 62

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.