FAQs durchsuchen



Data Center Expert | How do hardware and software support contracts work?
1 ) A Base software support contract is always needed and covers the base 25 nodes installed on the appliance.
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
1 ) ... be able to support the load attached ... ... is 20- 25 ... 4 years at 25 ... once every 6 months while in storage ... ... you're trying to support , please use ... A single piece of equipment ... In this application both input cords ... If one input cord is ... ... a UPS on one input and Utility ... You must only use the serial cable provided by APC with your UPS or an optional APC cable for your specific application . ... Serial cable is connected to the UPS, although no UPS shutdown software is installed ... A change of state causes the UPS to turn off.
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... 5. 1 .X and ... 1 .) Within ... 1 .a) ... ... is recommended you change the From Address Allow 1 -2 minutes ... ... that TCP port 25 is open. ... ISP's block port 25 since it has ... ... X do not support . ... be able to support SSL authentication. ... mail server, changing your From Address 1 .) Within ... 1 .a) ... If any one of the settings ...
Changing the language on the PowerView RM display (AP9215RM)
... How do I change the language on ... ... display can be changed by using the ... You can change the language by ... ... from the APC Support website. To change the user interface ... 1 . Remove the ... ... . Connect the programming cable (included ... ... connector of the programming cable to a ... ... connector on the programming cable. ... Locate the language program file to be ... Each language program file appears on ... ... the PowerView in programming mode by pressing ... ... will display the Programming screen. ... To leave the Programming screen before starting ... beeps (about one second).
Creating an Aggregate Device within the KVM Access Software
... KVM Access Management Software and why it ... KVM Access Software (ships with ... ... their KVM Access Software All software versions ... ports into a single Aggregate Device, ... counts as a single node, and only requires a single license. ... through the Access Software . When a ... ... the KVM Access Software . 1 .) Within ... ... you are adding one of the specifically ... ... how often the system automatically checks that ... ... information under certain single sign on situations ... ... click on the one (s) ... ... device does not support this function, ... ... device only has one network interface, ...
Changing the Language of the Symmetra PowerView RM Display
... I need to change the language displayed ... You can change the language by ... ... enclosed CD. Support for additional languages ... To change the language of ... 1 . Disconnect the ... ... . Connect the programming cable (included ... ... connector of the programming cable to a ... ... connector on the programming cable. ... Locate the language program file to be ... Each language program file appears on ... Program files for additional language support or code updates ... ... PowerView interface in programming mode by pressing ... ... will display the Programming screen. ... To leave the Programming screen before starting ... beeps (about one second).
How do I update/change the language pack on my Network Management Card 2 device?
... I update/ change the language pack ... ... These devices can support localization in up ... ... for updating/ changing these language packs which can change the language of ... Not all applications have language packs ... Only one language pack is ... ... Language packs are APP version specific - ... application for a Smart ... ... , please use one of the three 1 .) Open ... ... 2.) Change directories to the ... ... is necessary to change to the / ... 1 .) Identify ... application : ... 1 .) Refer to for instructions on upgrading firmware via USB. ... APP =apc_hw05_sumx_621.bin
Version 3 Netbotz modem support.
... 3 Netbotz modem support . ... and 500 families support modems. 1 . Mulit- ... 1 . Mulit- ... With the release of Botzware 4.2, some new modem support has been added. ... 1 . Zoom Model 4595 Modem (USB Stick form factor) ... Botzware 4.5.3 adds support for additional USB modem: ... Although we try to keep this document up to date, you can also verify changes to new releases i the release notes for the newest versions. This should be available on the product page or on the software downloads page:
Single Phase Symmetra UPS reports a Battery Discharged message
Single phase Symmetra PowerView display reports "Battery discharged" or network management card reports "The battery power is too low to support the load; if power fails, the UPS will be shut down immediately" ... This setting is configured for 2 minutes by default but can be changed depending on the amount of time needed to gracefully shutdown your servers when using PowerChute Network Shutdown (PCNS). ... If graceful shutdown software is not used, this setting can remain at its default of 2 minutes.
Does my APC network enabled device support RADIUS or LDAP?
... network enabled device support RADIUS or LDAP ... ... devices do not support LDAP, or ... ... party tools and software that will allow ... Some RADIUS servers allow integration with secondary authentication servers (LDAP as one possible example). ... Please refer to your software server vendor for information on integrating RADIUS into your security infrastructure. ... access to the APC networked device unless the Service-Type attribute is changed on the RADIUS server to allow administrative access. ... Please note that APC does not test and does not support nor recommend the applications listed or any comparable substitute that may be available.


Ergebnisse 1 - 10 von 75

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.