Consultar las preguntas frecuentes

Is there a kit available to convert from a NetShelter SX cabinet to a NetShelter SX Networking cabinet?

Fecha de publicación: 30 April 2019

Issue:
A customer is requesting a kit to change the rails of a NetShelter SX cabinet into the SX Networking cabinet.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
The customer may have purchased the wrong cabinet or their needs may have changed.

Resolution:
There is currently no kit available to convert a NetShelter SX cabinet into a NetShelter SX Networking cabinet. The rails are not sold separately. There are more differences between the SX and SX Networking cabinets than just the rails. For a complete overview of the differences please see Knowledge Base article FA158652.

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.