Consultar las preguntas frecuentes



How do I hardwire 10kva and 20kva transformers in a 208/120 or 240/120 environment
Please also make sure that the input voltage switch is in the correct position.
General Receptacle Wiring Practices
Generally a 120 / 208 volt , five wire system derived from a transformer with a wye secondary is used in commercial applications.
How to change the Input Voltage Select Jumper on a Symmetra Power Array
The jumper must be set to match the user's input voltage , either 208 or 240 VAC.
How Does Matrix-UPS Report Output Voltage?
The factory default for Out V Report is Auto; in this mode the Matrix-UPS reports its output with respect to its input voltage selection (set manually inside the UPS by the user at start-up). If it is desirable to monitor the voltage at a specific output receptacle, the choices are 208 and 240 VAC. The 240 setting is also useful for customers whose Matrix-UPS powers exclusively 120 VAC loads, their voltage is one-half the 240 VAC report.
Verification of Matrix-UPS input voltage configuration
... of the input voltage selector wire on a Matrix? ... be configured for a 208 or a 240 environment. ... UPS 3000 and 5000 units are wired ... the factory for a 208 Vac input. ... be used in a 240 Vac environment, the Input Voltage Select Wire must ... ... This document describes a procedure that can ... ... the input line voltage with the sub ... ... be near either 208 Vac or 240 Vac due to ... ... will either be a letter I or a letter M ... If there is a letter M
Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
... 240v loads from a 208v/240v ... ... do not require a stepdown transformer to ... ... outputs and require a transformer to supply ... ... UPS RT is a single phase UPS with a 3 wire unbalanced ... ... 2 hots and a ground on the ... 2 hots and a ground on the ... ... do not use a neutral. They require a stepdown transformer to ... loads and provide a Neutral ... you will see 208 volts (or 240v ... not two balanced 120 volt legs as you ... ... hardwire out to a 120v load without the use of a transformer will result ...
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
... do I configure a 208v Smart- ... for use with a 240v input? ... Online line has a very broad range of acceptable input voltages , and as ... ... order to avoid a sudden voltage shift in the ... ... be done via a Hyper terminal session ... ... Here we choose 240 VAC output and ... Output voltage will not change ... the UPS is left "on" ... ... UPS output is left on. If you need 120 v for your equipment you will still need to use a stepdown transformer. ... The following video demonstrates how to configure the output voltage of Smart-UPS Online SRT Series via the display:
APC Schneider Cooling Unit Identification
Voltage ... E= Expansion A = Air Cooled ... Economizer BA= 208 -230/ ... Voltage A = 3 row ... BA= 208 -230/ ... AA= 208 / 208 /3/ ... ... =480/ 208 /3/ ... ... =600/ 208 /3/ ... Voltage AA= 208 / 208 /3/ ... ... =480/ 208 /3/ ... ... =600/ 208 /3/ ... ... = No Humidifier A = In- ... Voltage AA= 208 / 208 /3/ ... ... =480/ 208 /3/ ...
Why does ISX Manager/StruxureWare Central display the incorrect Kilowatt value when utilizing the Physical Layout or ISX Operations feature for my Metered/Switched Rack PDU product?
... APC has identified a problem that causes ... ... firmware report their voltage and load to ... The problem that occurs stems from the Metered/or Switched Rack PDU and inline current meters reporting incorrect voltage . PDUs that operate on voltages , such as 208 , 230, and 240 volts , will actually report 120 volts .
Symmetra LX Spare Parts List
... can I find a list of commonly ... ... is to provide a user with a list of spare parts for servicing a Symmetra LX UPS ... ... Spare parts for 208 / 240 VAC Symmetra LX ... ... Castor kit - left front, right ... ... right front, left rear - SYAFSU7 ... APC Symmetra LX 5 U replacement door ... ... /230/ 240 /380/ ... Symmetra LX Castor kit - left front, right rear - SYAFSU6 Symmetra LX Castor kit - right front, left rear - SYAFSU7 ... APC Symmetra LX 5 U replacement door - SYAFSU1


Resultados 1 - 10 de 89

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.