Consultar las preguntas frecuentes



​How to read Modbus Status bits
Below is a couple of examples from a Galaxy VX : Example 1: Register 400002 (16385)
Modbus; How to read Status bits
Below is a couple of examples from a Galaxy VX : Example 1: Register 400002 (16385)
The “Generic Modbus” application does not provide status bits values in binary
Below is a couple of examples from a Galaxy VX : Example 1: Register 400002 (16385)
The “Generic Modbus” application does not provide status bits values in binary
Below is a couple of examples from a Galaxy VX : Example 1: Register 400002 (16385)
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
... of new Galax VX or Galaxy VM. Galaxy VX , Galaxy VM ... first logging into a network device. ... display of the Galaxy VX and VM is ... Use a terminal program with ... ... 9600 bps, 8 data bits, no parity, 1 stop bit, ... ... asked to enter a new password. Open a browser and enter IP Address; example address ... At the bottom of the screen you will a box to enter a password for “Pin [4- 8 digits]” and a “Confirm Pin 4- 8 digits]” and click on Save button.
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
2.) Utilize an APC ap9600 single slot SmartSlot expansion chassis and extend the cable to the ap9600 with a 940- 1500 serial ...
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... Powering Down the Galaxy 5000 UPS This procedure is for a single UPS with an external maintenance bypass panel. ... Step 1 : Touch any button on the display to wake it up. ... Step 5 : Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch. ... Step 8 : Unlock CB2, remove the key, and place it in the key interlock. ... Turn off Q 1 Switch
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... reasons, the Galaxy 5000 may be in a totally off state ... ... not for commissioning a new UPS. ... The commissioning of a new UPS must be performed by a Schneider Electric trained ... How to restore the Galaxy 5000 UPS from total power off to normal operation. This procedure is for a single UPS without an external bypass panel. ... Step 1 : Set the input Q 1 switch to On ... Step 5 : Turn the Q4S Switch to On ... Step 8 : Set the battery circuit breaker(s) QF1 to the On Position.
Information regarding the Aluminum cable for the Galaxy VX products
Information regarding the Aluminum cable for the Galaxy VX products. ... All Galaxy VX 1250 KW, 1500kw ... Recommended Aluminum Cables for 1250kw – 1500 KW
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
... apcmedia.com/salestools/MBPN-A35JB8/MBPN-A35JB8_R 1 _EN.pdf?sdirect=true


Resultados 1 - 10 de 68

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.