What is Modbus and How does it work?
... is represented by one of the 256 ... ... or contact is 1 bit and assigned ... ... Each register is 1 word = 16 bits = 2 ... 1 , 10001, ... ... is assigned a unique unit address from 1 to 247. If even one bit in the ... ... converts to the 16 bits ... any of these 16 -bit data ... 16 -bit unsigned ... 16 -bit signed ... ... the same as 16 -bit integers ... of 0 or 1 . = - 1 ,371, ... ... accuracy of about seven digits. ... = ® A V R the higher 16 bits (high ...