Consultar las preguntas frecuentes



Shutdown VMware ESXi 4.X, 5.X unlicensed server with PowerChute Network Shutdown
Issue: How to shutdown VMware ESXi host that is running the free edition of VMware with PowerChute Network Shutdown
PowerChute Network Shutdown 2.2.4 and 4.5G and 5G Smart UPS Behavior
When using Powerchute Network Shutdown 2.2.4 and Network Management Card 2 ... the UPS via PowerChute Network Shutdown is supported for only ...
Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) Device between v5.X.X and v6.X.X
For users using APC PowerChute Network Shutdown software, a new "PCNS User Name" setting must be configured along with the existing authentication ...
The ESXi host running the free edition of VMware is not shutting down when commanded to by PowerChute Network Shutdown.
If PowerChute is running on ... .1 or 5 .x please ... commanded to by PowerChute Network Shutdown running on 4.1 & 5 .x. ...
What to do if PowerChute Network shutdown configuration wizard displays blank Network Configuration page?
5 - Restart PowerChute service from command prompt type net start PCNS1
Configuring Virtual Machines to shut down when a Hyper-V host is commanded to shut down.
For PowerChute Network Shutdown v3. ... and above, steps 5 and 6 are ... enabled the VM shutdown option in PowerChute when Hyper- ...
Host running vCenter Server virtual machine (VM) is not commanded to shut down when PowerChute Network Shutdown is also deployed as a VM.
vCenter Server 5 .x installed ... vCenter Server Appliance 5 .x, ESXi 5 .x , PowerChute Virtual Appliance or PowerChute installed on vMA ...
PowerChute Network Shutdown Configuration Files Explained
Prior to version 3.x of PowerChute Network Shutdown (PCNS), configuration data was stored in a proprietary binary file.


Resultados 1 - 10 de 84

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.