Consultar las preguntas frecuentes



What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6H?
Cause: A 15 A fuse is installed in the circuit, but the connected load requires the use of a 20 A fuse.
What are the basic troubleshooting steps for the Universal Transfer Switch model uts10bi?
Cause: A 15 A fuse is installed in the circuit, but the connected load requires the use of a 20 A fuse.
What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6 / UTS6BI?
Cause: A 15 A fuse is installed in the circuit, but the connected load requires the use of a 20 A fuse.
SYTF2 for use with Symmetra RM with 208vac Input and Output only
... on the windings of this transformer, he NEMA 5-15 120vac outlets on the rear of the SYTF2 will supply 120 VAC only ...
NEMA 5-15 receptacle description
Resolution: The NEMA 5-15 receptacle is the most common electrical receptacle in the United
No power output from the Matrix-UPS L14-30 or 5-15 receptacles (mx3000/5000)
... UPS output to the L14-30 receptacle (as well as the NEMA 5-15 receptacles on the Matrix-UPS 3000 model ...
What are the standard output receptacles for the Matrix UPS line?
The Matrix comes standard with (6) 5-15 receptacles, (2) L6-30 receptacles and (1) ...
Can I change the input power plug on my 120vac Smart-UPS?
Cause: All Smart-UPS 2000va or larger have an input plug that is not a standard 5-15 household style plug.
Smart-UPS C Series FAQ
Domestic units solid in North America use NEMA 5-15 plugs for input and output.
Where can I get support for APC and MGE Products?
... 1 0034- 100 0034-3 0035- 100 0035-2 ... E 0039- 15 0040-10 0040- 15 0082- 15 0082-25 ... E 0226- 15 0226-25 ... ... 12 0386- 15 0389- 8 0414-10 ... 25 0422- 100 0422- 15 0422-35 0423- 15 0423-25 ... 25 0465- 100 0465-25 ... 20 0473- 15 0474-10 0474- 100 0474- ... 100pk 0857- 100 0857-50 ...


Resultados 1 - 10 de 53

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.