Consultar las preguntas frecuentes



Does my Smart-UPS have Equipment Protection Policy (EPP) coverage?
Any unit installed outside of the U.S. or Canada
Galaxy 5000, Galaxy 5500; Dust Covers
MGE Galaxy 5000, Galaxy 5500, Dust Cover, Input Wiring, Installation , foreign conductive particles,
Whether to install a suction line drier or liquid line drier
Installing a suction line drier in an ACRP DX is a tight fit, but possible. The obvious benefit of a suction line filter drier is the added protection given the system if a burnout should occur. The filter will effectively prevent contamination resulting from the failure from traveling back through the suction line into the other parts of the system. This will minimize the contamination remaining in the system when the inoperative compressor is removed. With this said, it is preferred to put the drier in the suction line. If a technician cannot find a suitable suction line drier with replaceable cores to fit inside the ACRP, a liquid line drier would be fine. It is ok to use an additional liquid line drier with replaceable cores. This can be handy since a technician will have more room on the outside liquid line to install isolation valves to keep the downtime to a minimum when replacing cores. The ACRP uses Danfoss liquid line drier pn # 023z4581, 5/8" ODF SOLDER. You will need to find a small suction line filter drier. After the cleaning procedure is completed, recheck in approximately one to two weeks to ensure that the system condition and operation is completely satisfactory.
Is there a depth extender for the rear or front of NetShelter SX cabinets? Is there a way to bay the rear of cabinets that are different depths?
The EcoAisle product line offers depth extenders. They can also be used outside of an EcoAisle installation .
What is the proper method to secure a NetShelter SX to the floor, and what are the bolt patterns?
... mounting bracket and ar7701 Bolt-Down Kit in the illustrations below are installed both inside and outside of the cabinet.
What are the requirements for the acsc100 condenser unit
acsc100, duct, condenser temperature, install , discharge, outside
PowerChute Network Shutdown shuts down an ESXi host in vSAN cluster before it has been moved to maintenance mode.
All servers are protected by 1 UPS PowerChute and vCenter Server are installed on a physical server outside the HA cluster


Resultados 1 - 10 de 97

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.