Consultar las preguntas frecuentes



Serial Terminal Connection Parameters for all NetBotz Appliances
When connecting to models 355, 455, 550, 570 or similar version 3 Netbotz, you must use a USB A- B cable. The NetBotz 200 uses a Null Modem cable and a baud rate of 9600.
NetBotz 750 | Resetting a Lost Root Account Password
1) Connect a USB-A to Micro USB- B cable to the Console Port on the NetBotz appliance and a USB port on your computer. ... Baud: 115, 200
Video: Using Network Management Card 2 (NMC2) bootmonitor to recover/upgrade firmware
Appendix B . ... CPU Speed : 200 ... CPU Speed : 200 ... CPU Speed : 200
APC Security Advisory - Static Factory Password Vulnerability
... _aos_ 200 .bin) ... B . If a console port server is connected to a vulnerable product's local serial port then ensure that the console port server forces user authentication prior to allowing login to the product. ... B . If a console port server is connected to a vulnerable product's local serial port then ensure that the console port server forces user authentication prior to allowing login to the product.
What are some features I need to be aware of while manipulating the config.ini file of a APC Network Management Card?
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (ap9320, ap9340, Netbotz 200 ) ... =00 C0 B 7 6A 33 56
Video: How do I configure APC Network Management Card network settings?
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (ap9320, ap9340, NetBotz 200 ) ... All APC devices have a MAC address that begin with 00 C0 B 7 ... You may want to check your DHCP client list for any MAC addresses beginning with 00 C0 B 7, which indicates an APC address.
ACSC1XX Spare Parts List
DIVIDER-' B ' DUCT KIT ACSC 5KW 48ECT BC NKRAFT ... Pwr Cord, 16A, 200 -240v, C19 to L6-20 ... 1U 19" Black Modular Toolless Airflow Management Blanking Panel - Qty 200
What is the transfer time of the Back-UPS?
The transfer time of the BK CS and ES units is 10-12 milliseconds.
What are some issues I may encounter when using an APC Back-UPS with a generator?
support this functionality. Legacy model Back-UPS products (such as the BK series) may not support this functionality.


Resultados 1 - 10 de 50

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.