Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
Hardwiring to 120v, 208v ... These two models are split ... a stepdown transformer to support 120v loads ... ... require a transformer to supply 120v loads ... They require 2 hots and a ... input, and 2 hots and a ... ... a stepdown transformer to power 120v loads ... ... that from hot to hot you will see 208 volts (or 240v ... it is not two balanced 120 volt legs as you ... The two output legs are ... and from hot to hot they will ... ... these units default to 208v out and can be configured to 240v via the ...