Consultar las preguntas frecuentes



Why won't my Lithium-Ion Smart-UPS start when the battery is first connected when there is no utility power to the unit?
... then there will be up to a 1 minute delay between the initial connection of the battery and the UPS being ready to start .
APC Recall for the Back-UPS CS (120v and 230v); How do I know if my unit is one of the affected units?
Environment: Only units with serial numbers having the first six characters that fall between the following ranges are affected; excluding
How can I adjust the number of battery packs on a Smart-UPS XL?
... how many external batteries are connected so ... ... : Models that begin with SMX are ... can use external batteries . ... and have Smart Batteries . battery packs. battery packs. batteries effects the runtime ... ... is running on battery power. ... number of external batteries . 1 . Using Hyperterminal ... external battery packs ... the number of battery packs via a ... 1 . First , EXIT out ... ... go to: Start |Programs | ... ... data bits, 1 stop bit, ... 6 . Click OK ... ... " Adds a battery pack ... number of external battery packs ... " Subtracts a battery pack
What is the functionality of the Power On/Off Button on my CSH2 Smart-UPS Charge Mobile Battery for Microsoft Surface Hub 2?
... UPS Charge Mobile Battery for Microsoft Surface ... ... UPS Charge Mobile Battery for Microsoft Surface ... 2 features a single On/Off ... Power On/Off functionality ... up automatically and starts charging the battery . ... due to low battery condition, then ... charge of the battery is > 30 ... ... • Wakeup on battery • Cold start on battery ... and less than 6 seconds to enable ... white indicating the battery state of charge ... ... and less than 6 seconds to enable ... ... white indicating the battery state of charge ... ... for more than 6 seconds and less ... : Press the POWER ON/OFF button for more than 3 seconds and less than 6 seconds to reset the alert.
Frequently Asked Questions for the new Lithium-ion Smart-UPS products.
The UPS has a unique internal battery connector to avoid any misconfigurations in the field.
Troubleshooting steps to perform when "Please check that the USB cable between your battery backup and PC is properly connected" message or "Unknown Device" appears after a reboot of your computer.
... cable between your battery backup and PC ... ... the following APC Battery Back-UPS ... 1 . Ensure that ... ( Start - Settings - ... 6 . Once the ... ... see listings as Batteries and Human Interface ... 10. If other USB devices are connected to the PC disconnect these devices before connecting the UPS USB cable and retry steps 1 -8. ... 11. Reboot your PC. After reboot, did your PC recognize the UPS or are you still receiving the initial message of ""Please check that the USB cable between your battery backup and PC is properly connected""?
Video: Battery Installation of APC AV Power Conditioners with Battery Back-Up
... and connect the battery in a APC Power Conditioner with Battery Back-Up at first time start -up or following routine battery replacement. ... Power Conditioners with Battery Back-UP Battery must be installed ... ... of-life battery . ... with the internal battery pack disconnected. ... connection of the battery when the front ... ... Connect the internal battery pack as follows ... 1 . Grasp the ... ... . Push the Battery Wire Connector ( ... left of the Battery Pack. ... Ensure that the Battery Wire Connector is ... ... . Install the battery retaining bar.
Why are the battery charge LEDs flashing on a Smart-UPS?
Battery Charge LED Bar ... ... model numbers that begin with SU, ... ... than the low battery signal warning time ... ... than the low battery signal time, the battery charge graph LEDs ... Option 1 : ... Reset the low battery signal time to ... ... with the low battery signal warning time ... ... , then the battery bar graph LEDs ... ... setting the low battery signal warning time ... ... , the low battery signal time is ... UPS battery ... or replace the battery . ... , yet the batteries are consumable items ... As the batteries age, they ...
How to Cold Start a Symmetra LX Extended Run Frame
The extended run frame needs to have at least one good battery installed with the black knob on the front of the battery in the ...
Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003
Step # 1 : ... 2000 Click on Start > Settings > ... ... 2003 Click on Start > Control Panel ... ... is set to start manually. ... UPS service will start on bootup. ... select button to begin configuration. Note 1 : 1 Stop Bit ... new settings and start the UPS service ... Step # 6 : ... as Runtime, Battery Capacity and battery condition. The first check box is ... Here you can choose how long after the UPS switches to battery that you will receive the first notification. ... The second checkbox sets the amount of time the system will run on battery before a critical alarm” state is reached.


Resultados 1 - 10 de 99

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.