{"searchBar":{"inputPlaceholder":"Busca por palabra clave o haz una pregunta","searchBtn":"Buscar","error":"Ingresa una palabra para buscar"}}
{}

Nuestras marcas

{"support":{"yesButton":"Sí","noButton":"No","feedback":{"title":"¿Qué podemos hacer para mejorar?"},"submitButton":"Enviar","successMessage":"Gracias por tus comentarios","title":"¿Te fue de ayuda?","feedbackPercentLabel":"de las personas encontraron esto útil","captcha":{"error":"Por favor, marca una casilla"}}}
Buscar Preguntas Frecuentes

The ESXi host running the free edition of VMware is not shutting down when commanded to by PowerChute Network Shutdown.

Issue:
VMware ESXi host, which is running the free edition of VMware, is not shutting down when commanded to by PowerChute Network Shutdown.

Product Line:
PowerChute Network Shutdown (PCNS) version 2.2.3, 2.2.4, 3.0, 3.0.1, 3.1, 4.x

Environment:
VMware ESXi versions 3.5, 4.x, 5.x, 6.x, 7.x

Cause:
The free edition of VMware ESXi provides read-only access to the API functions. Without write access to the API functions, PowerChute cannot issue a command to shut down an ESXi host.
To review a list of supported VMware ESXi versions see What VMware ESXi Licenses are support with PowerChute?

Resolution:
To make PowerChute Network Shutdown work properly you will need to purchase a license for ESXi. 

You can also find more information in Kbase Shutdown VMware ESXi 4.X, 5.X unlicensed server with PowerChute Network Shutdown

 

¿No encuentras lo que estás buscando?

Comunícate con nuestro equipo de Atención al Cliente para recibir soporte técnico, asistencia para quejas y más.