EcoBreeze Variable Speed Drive Technical Spec’s
Line current 71.9 ... ... 28.5 kVA Maximum transient current 99 A for ... Continuous output current 66 A at ... Transient overtorque 150 ... ... ... braking resistor continuously 150 % without braking resistor ≤ 150 % with braking ... ... Ohm AI3 configurable current 0.. ... ... type AOC configurable current 0.. ... Minimum switching current R1- ... Maximum switching current R1- ... Vibration resistance 1 gn (f = 13... 150 Hz) conforming to EN/IEC 60068-2-6 1.5 mm (f = 3.. ...