Does the NetShelter VED Kit provide cooling?
... if the VED Kit provides cooling. NetShelter VED Kit ... the ceiling to recirculate back to a ... Servers and IT equipment have their own fans which force hot air to the back of the cabinet. If there is no larger AC unit drawing that hot air from the cabinet into the VED, then into the plenum, it might be advisable to incorporate an ARU (acf400, acf402) instead of a VED.