How to navigate through an Network Air FM unit display
Operation . ... MultiCool® ( chilled water) and ... ... near the environmental sensors , and is ... ... , then the cooling setpoint is used ... ... when the remote sensor readings are used ... ... the next time power is applied to ... ... avoid over- cooling while dehumidifying. ... the modes ( cooling , reheat, ... ... System cannot begin operation until this delay ... ... It allows the sensors to obtain an ... Sensor setup ... System Config > Sensor Setup ... the set of sensors the Module will ... ... temperature and humidity sensors the controller will ... The return sensors and the remote sensor string are available ...