Browse FAQs



What width cable ladder will attach to the pass-through data cable partitions?
If you have cable ladder that requires attachment hardware please see sku AR8166ABLK Cable Ladder Attachment Kit . .
What is the capacity (in Lbs.) of NetShelter Cable Ladder, or the capacity of a structure containing cable ladder?
Information regarding the capacity of NetShelter Cable Ladder is required. ... NetShelter Cable Ladder ... See attached file
InfraStruXure™ InRow Data Cable Bridge Partition, 300 mm Wide—acac10005
Issue: This document describes how to install a InfraStruXure™ InRow Data Cable Bridge Partition , 300 mm Wide—acac10005.
How to install InfraStruXure™ InRow Data Cable Bridge Partition, 600 mm Wide—acac100010
Issue: InfraStruXure™ InRow Data Cable Bridge Partition , 600 mm Wide—acac100010.
Is there a NetShelter Accessory Compatibility Chart that shows which NetShelter accessories, UPS, PDU, Symmetra, NetBotz, Air or KVM fit into a specific cabinet?
... door, doors, vertical, horizontal, cable manager, management ... , manager, ladder , shelf, trough, partition , bracket,
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... Rack Expansion Bundle Kit next to a ... ... from APC. Attach the ground strap ... 1. Attach two trim brackets ... ... °, and attach it to the ... °, and attach it to the ... ... support power or data cables ... installation of the ladders . 2. Attach the next ceiling ... To attach the door frame ... 1. Attach the door frame ... 3. Attach the plinth blocks ... Attach one end of ... , and then attach the other end ... ... an optional grounding kit (ar8390) ... ... new equipment for information on installation, ... APC offers an optional grounding kit (ar8390) for grounding an enclosure Data Troughs
Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
... AR8561 may also be used to span the cooling unit but they can not be attached directly to them.
Changing the Language of the Symmetra PowerView RM Display
c. Attach the UPS data cable to the female RJ-45 connector on the programming cable .
What is the maximum cable bundle diameter allowed by the the AR8621 Toolless Hook & Loop Cable Manager, and how long are they?
Issue: This information is needed to determine what size cable bundles can attach to each AR8621.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.