Browse FAQs



Matrix-UPS run time theory
... method the Matrix UPS calculates its estimated ... Matrix UPS ... on the Matrix UPS calculates the " ... " based on five variables: 1 . Age of ... 5 . Percentage of ... applied to the UPS . ... time the voltage levels off for a ... ... To allow the UPS to predict when ... ... curve, the UPS will be able ... ... at 40 volts DC the batteries are ... If the UPS load is too ... that when the UPS is on- ... When the UPS is first installed with a ... ... Hex) the UPS might begin a ... ... KBase document titled "Requirements for Matrix UPS " ...
Video: Troubleshooting no communication between UPS and PowerChute Business Edition
... No Communication with UPS Troubleshooting Windows Serial Communications ... for Smart- UPS models SU, ... ... the "Checking UPS Communications on Windows ...
How do I properly install/uninstall my SmartSlot accessory card into my UPS?
... into my APC UPS ? APC UPS Models - Single and Three Phase including Smart- UPS and Symmetra models Device UPS Management accessories including ... UPS Network Management Card 1 and 2 Interface Expander 1 /2 ... card while the UPS unit is in ... The first six characters should ... ... depending on your UPS type. Smart- UPS (SU, ... ... connected to the UPS Disconnect the UPS from its AC ... ... to turn the UPS off. ... button for approximately five seconds to turn off the DC (battery) ... ... then plug the UPS back in and ...
Video: How do I configure APC Network Management Card network settings?
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... , Smart- UPS Online (SRT ... ... Network Management Card 1 : ... Network Management Card 1 (AP9617, ... Network Management Card 1 (such as ... ... Network Management Card 1 based devices are ... ... device, select one of the available ... Smart- UPS front panel LCD ... Configuration Option 1 - Device IP ... ... program, any services using the COM ... ... , the APC UPS service must be stopped ... ... with an APC UPS or accessory.
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... Environmental Monitoring Unit 1 (AP9312TH) ... ... Network Management Card 1 - AP9617, ... ... Network Management Card 1 include (but ... ... , Smart- UPS Online (SRT ... ... device from v 5 .X. ... ... installed in a UPS , you need to determine which UPS you have. ... offers several different UPS families. Smart UPS Symmetra 1 phase (Symmetra ... ... Select the correct UPS or device type ... and select UPS Network Management Cards ... have a Smart UPS 750 (sua750 ... UPS Network Management Card ... for Smart- UPS and Matrix w ...
Why can it take PowerChute Business Edition Agent 5 minutes to establish communications with the UPS?
After the PowerChute Business Edition Agent starts (signalled by the "Monitoring Started " event in the Event log), it sometimes takes 5 minutes before UPS Communication is established. ... PowerChute Business Edition v10.0. 1 , v10.0.2, v9.5 and previous versions communicating with Smart- UPS SMT, SMX, SURTD. ... This issue is caused by certain combinations of UPS and PowerChute Agent software.
Video: How to Start your Silcon UPS
How to Start your Silcon UPS ... The first step is to return utility power to the ups by turning the Q 1 switch on. ... “Stop Charge DC Capacitors: Yes” ... Start Charge DC Capacitors: Yes” ... UPS is now started . To take the UPS out of Maintenance Bypass do the following. Start by putting the ups into Static Bypass by pressing the # key ... The UPS is now out of Maintenance Bypass
SRT 8 or 10kva reports Error P.11 or DC Bus Soft Start or event codes 124/125
The UPS reports P.11 or DC Bus Soft Start - event 124/125 ... If the problem persists, Brain dead the UPS . If the alarm reoccurs, perform a UPS Firmware upgrade to the latest 04.7 revision that addressed these issues. ... Release Notes ( UPS 04.7): ... 1 . Improved system performance of transitions between Online and Bypass operation modes. ... 3. Improved system behaviour to eliminate false detection of DC bus under voltage alarm under certain conditions. 4. Improved system handling for certain AC input conditions during system start -up.
Video: How to perform a cold start and brain dead on Smart-UPS
... perform the Cold Start and Brain Dead ... Smart- UPS The Cold start procedure is used ... determine if a UPS is functional if ... ... the Smart- Ups microprocessor. Cold Start : ... establish if a UPS will not turn ... ... use a Cold Start to troubleshoot a ... 1 ) Turn off ... the Smart- UPS from wall. ... front of the UPS until you hear ... 4) UPS should go through ... ... shows that the UPS is functioning correctly ... 5 ) You can now plug your UPS back into the ... ... is acceptable the UPS will transfer back ...
How can I adjust the number of battery packs on a Smart-UPS XL?
Smart- UPS XL products require ... you tell the UPS how many external ... so that the UPS can properly calculate ... Smart- UPS XL Smart- UPS XL models are ... Smart- UPS XL models are ... ... a Smart- UPS performs when it ... the Smart- UPS XL to recognize ... 1 . Using Hyperterminal ... 1 . First , EXIT out ... the UPS service must be stopped ... ... go to: Start |Programs | ... ... data bits, 1 stop bit, ... 5 . Click on ... ... with an APC UPS or 1 . Unload the ... ... com port the UPS serial


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.