Browse FAQs



What are the operational conditions for an InRoom (Stulz) Unit
... °F) Upper limit : Depending on ... 460v / 3ph / 60 Hz ... -230v / 3ph / 60 Hz Chilled water-/ cooling water pipes: Maximum water head pressure ... Maximum equivalent length of piping between the cooling unit and the ... Maximum level difference between the condenser and the cooling unit: 5 m (16 ft) when the condenser is below the cooling unit ... Maximum condensing temperature: 60°C (140°F) Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol Data is valid for: 460v / 3ph /60 Hz
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... acrc301h, acrc301s Cooling Units, ... future firmware update plans to address this ... ... acrc ACRCXXXX InRow Chilled Water (except ... ... your local APC Cooling Support team) ... ... your local APC Cooling Support team) ... ... your local APC Cooling Support team) ... (via your local APC Cooling Support team) nb200 NetBotz 200 Rack Monitor (nbrk0201) ... sumx 1ph/ 3ph Smart-UPS, MGE Galaxy 3500, Matrix AOS v6.4 and higher Yes
Utilizing the maximum output capacity of the Symmetra RM 6kva
... Symmetra RM to be utilized to a capacity greater than 5kva, the input to the unit should be hardwired to 40 amp service in ...
APC Schneider Cooling Unit Identification
IEC-309 16 A 4-wire ( 3PH + G) (13.737 kW input)
When polling dual registers in InfraStruXure Central 6.0, both registers must be polled together.
Because some values returned by ISXC may be greater than this maximum value, we have created the ability to use 2 registers together as ...
Where can a NetShelter CX be deployed?
... offices with no air conditioning - Larger sizes of NetShelter CX with maximum thermal load will potentially require additional cooling assistance from an open window ...
What are some of the applications for the InRow ACRD?
... handling low loads of 2-20kw which makes it a great choice for customers with long term growth plans .
Why is my ACRP excessively cycling?
The cool setpoint controls the fan speed based on the maximum rack inlet temperature.
PowerChute Network Shutdown version 4.1 web interface is not accessible after installation on Solaris 10 and 11
java.lang.IllegalStateException: Insufficient max threads in ThreadPool: max =200 < needed=XXX (where XXX is greater than 200)
How to acces the Overview Status of an ACRD6XX/ACRD6XXX
Operating Mode, Max Rack, Fan Speed ... Temp, Return Temp, Cool Output, Cool Demand acrd600, acrd600p, acrd601, acrd601p


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.