Browse FAQs



Video: What does the Site Wiring Fault Indicator LED on my APC UPS or Surge Arrestor represent?
All 120v APC Back-UPS and SurgeArrest products ... -UPS and SurgeArrest products equipped with ... ... only present on 120v UPS and Surge ... If the outlet that the APC UPS unit is plugged into is not properly grounded or properly wired, the unit will attempt to absorb the excess voltage instead of redirecting it to ground. ... Therefore, in order to maintain your warranty and protection under APC's Equipment Protection Policy, be sure that the APC unit is only plugged into a properly grounded outlet where the Site Wiring Fault Indicator (SWF) light is not illuminated.
Video: Data Center Expert | Backing up to a Windows Share
DCE backups should be performed on a regular basis. ... Performing a Backup within DCE ... 4) Add the specific user that you would like DCE to use to connect for storing the backup. ... 11 ) Select Apply and OK. ... You will need the share name, IP address of the windows system the share is stored on, and the credentials for the user you granted full control. Performing a Backup within DCE ... - Security : On Data Center Expert version 7.3.1 and higher, the share security can be defined.
Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
... Certain Audio/ Video Network Management Enabled ... 2.) Change directories to the directory that you want the files stored in. ... *If using Network Management Card 2 only, files are now stored in the /logs directory on the card. ... 11 .) Optional: ... Connect to the card via FTP or Secure CoPy.
Where can I get support for APC and MGE Products?
Biometric Security ... Metered-by- Outlet Rack PDU ... Notebook Security ... Operations Energy Efficiency ... Security Cameras ... SurgeArrest Essential SurgeArrest Home/Office SurgeArrest Notebook SurgeArrest Performance
Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?
illuminate: 1. The unit is powered off (for 7 outlet SurgeArrest strips only).
Video: How to add PowerChute security certificate to Microsoft Internet Explorer 11
Solution: Add the PowerChute web security certificate to Microsoft Internet Explorer 11
Video: How can the Galaxy VS reduce my energy bill?
Enjoy the highest energy savings available today without sacrificing load protection – our patented zero-break transfer design offers peace of mind:
Proper installation of a telephone line into an APC product with telephone line protection.
1. Attach one side of a telephone patch cable to the telephone jack in the ... ""Wall outlet "" or be denoted ...
SurgeArrest - minimum install distance of 10 meters (30ft).
... between the electrical outlet and the electrical ... ... utilization equipment being protected . ... external short circuit protection . ... to the voltage protection rating Type 1 and Type 2 rated surge protection devices are additionally tested to UL96A "Lightning Protection Systems" specifications, as they are at or before the electrical service entrance. ... A Type 3 surge protection device is not intended for direct lightning protection , therefore it is tested beyond the potentially effected area. ... Ideally for residential use, Type 2 which is often referred to as "TVSS" protection should always be installed at the main electrical service entrance.
Recommendations for protecting a laser printer
What are APC's recommendations for protecting Laser Printers? ... SurgeArrest , Back-UPS and Back-UPS PRO ... Due to the large amount of power consumed by these devices, APC does not recommend protecting laser printers with a UPS. ... The Laser Printer should not be plugged into a UPS's Battery Outlets OR in to its Surge Only Outlets . These low voltage situations may cause an APC Back-UPS to transfer to battery operation repeatedly, eventually exhausting the unit's internal battery unnecessarily.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.