Rack PDU 2G (AP8XXX) Network Port Sharing Information
... AP8XXX Rack PDU models ... ability to share one IP address via one network connection) ... PDUs using only one ... a number, 1 to 4, ... After two or more Rack ... are connected to one another in a ... You'll need two terminators per Network ... ... which includes qty 2 terminators and provide ... ... " port of one of the grouped ... ... desired order, 1 to 4. ... ... have Display ID 1 . ... have Display ID 2 . Continue in ... ... power for phase 2 on guest Rack ... ... phReading 3: 2 power 2 : 40 W ... Group Status" page , and the ...